2014/09/30
 
 
 
Home > Manufacturers > Raspberry-Pi > Compute Module Development Kit
Share   Share on Facebook Share on Twitter Share on Google Plus Share by Email
Raspberry Pi

Raspberry Pi Compute Module Development Kit

The Raspberry Pi Compute Module devkit will enable design engineers to harness the power of the Raspberry Pi within their own embedded applications.

  • Raspberry Pi Compute IO Board
  • Raspberry Pi Compute Module
  • Raspberry Pi Display & Camera Adapter
  • Micro USB Power Supply (multi-regional)
  • Micro USB Cable and 4 x Jumper Wires
Raspberry Pi Compute Module Development Kit

Product Description

The Raspberry Pi Compute Module development kit will enable design engineers to harness the power of the Raspberry Pi within their own embedded applications.

Each kit is supplied with a Compute Module, an IO Board, adaptors to convert the CMIO board camera and display interfaces to use the official Raspberry Pi Camera (and display when available later this year), 5V power supply and a micro USB cable for flashing the eMMC from a host PC.

The Raspberry Pi is now contained within a small SODIMM-style 6.5x3.5cm module. This contains the BCM2835 chip, 512MB RAM and an on-board 4GB eMMC flash memory for booting the Raspbian operating system. This will connect into a custom peripheral interface board designed by the engineer.

To support the development of such custom baseboards, a fully functional IO board is provided as part of the Raspberry Pi Compute Module Development Kit which supports an extensive GPIO and multiple connectors to help foster rapid prototype development to help define the next generation of the “Internet of Things”.

It should be noted that this Compute Module is intended for serious design engineers interested in developing Raspberry Pi technology into their embedded projects, rather than consumers or hobbyist developers who require a significant amount of support to develop their own solution.

Small and powerful

SODIMM-sized (6.5cm by 3cm) Raspberry Pi board containing the BCM2835 chip with 512MB RAM along with an on board 4GB eMMC Flash memory for booting the operating system.

Rapid prototype development

The 200-pin edge connector provides the design engineer with access to all of the BCM2835 functionality. A fully functional motherboard is provided as part of the Compute Module Development kit which supports an extensive GPIO and multiple connectors to help foster rapid prototype development.

Bespoke solutions

Benefit from the dedicated hardware design created by an engineer, whilst still providing all of the power of a fully functional Linux application server to perform the analysis and computational tasks necessary to manage and self-diagnose the industrial solution. This unique combination of services will help define the next generation of the “Internet of Things”.

 
 
   

Feedback Survey

When you are done with your visit to our site, please fill out our feedback survey.

Start the Survey Now! no thanks[x]
powered independently by Qualtrics