NEW Improved CadSoft EAGLE
Version 7
Cadsoft has brought out the new improved seventh version of its award-winning EAGLE software for PCB design.
- Improved Autorouter
- Hierarchical Design
- GUI Makeover

Product Description
Cadsoft has brought out the new improved seventh version of its award-winning EAGLE software for PCB design.
EAGLE has offered the high level functionality of expensive commercial circuit board design software at a fraction of the cost for over 25 years.
EAGLE offers three modules - Schematic-Editor Layout Editor and Autorouter - embedded on one single interface. It runs on Linux Mac and Windows and allows feature enhancement such as simulation 3-D visualisation data import and export and self defined commands through User Language Programs (ULP's) which are partly integrated in EAGLE and available at the download area.
Autorouter
The existing autorouter is based on a rip-up retry algorithm in which it takes into consideration that parameters defined in Design Rule Checker and NetClass. This is a single thread process by which the end user needs to run the autorouter multiple to test different configuration. The new autorouter for v7 augments the existing algorithm. One of the most noticeable effects of the new autorouter is that it is Multi-Threaded and therefore can take advantage of Multicore processors.
Multi-Threaded
This means that the autorouter can run multiple configurations simultaneously. The user will be able to select the best outcome that accommodates his design. On computers with multiple core processors each thread can own its own processor core. This optimises EAGLE's use of the available hardware.
TopRouter
The new autorouter includes the option to use our TopRouter. This intricate process will result in boards with significantly less points of transition compared to our previous algorithm. This will result in very cost effective optimal boards that will need less manual interaction by the end user.
Autorouter
The existing autorouter is based on a rip-up retry algorithm in which it takes into consideration that parameters defined in Design Rule Checker and NetClass. This is a single thread process by which the end user needs to run the autorouter multiple to test different configuration. The new autorouter for v7 augments the existing algorithm. One of the most noticeable effects of the new autorouter is that it is Multi-Threaded and therefore can take advantage of Multicore processors.
Multi-Threaded
This means that the autorouter can run multiple configurations simultaneously. The user will be able to select the best outcome that accommodates his design. On computers with multiple core processors each thread can own its own processor core. This optimises EAGLE's use of the available hardware.
| Beschreibung | Kaufen | |
|---|---|---|
| CadSoft EAGLE Version 7 | Sortiment mit über 120 Produkten | Jetzt kaufen |