Raspberry Pi Boards


All the Raspberry Pi board models available to buy from the officially licensed manufacturer and distributor.

Primarily designed to help children and adults to enhance their skills in programming and digital literacy, Raspberry Pi devices are small, low-cost yet powerful computers around the size of a standard credit card. They are capable of running a number of coding languages including Scratch and Python, and can perform practically any function you'd expect of a desktop computer.

At Farnell, we offer an extensive selection of Raspberry Pi products, including the powerful Raspberry Pi 3 Model B+ and the Raspberry Pi Compute Module, capable of being applied to a wide range of projects from simple educational tools to complex design challenges.

Raspberry Pi 3 Model A+
512 MB RAM

The Raspberry Pi 3 Model A+ is the latest product in the Raspberry Pi 3 range. Like the Raspberry Pi 3 Model B+, it boasts a 64-bit quad core processor running at 1.4 GHz, dual-band 2.4 GHz and 5 GHz wireless LAN, and Bluetooth 4.2/BLE.

The dual-band wireless LAN comes with modular compliance certification, allowing the board to be designed into end products with significantly reduced wireless LAN compliance testing, improving both cost and time to market.

The Raspberry Pi 3 Model A+ has the same mechanical footprint as the Raspberry Pi 1 Model A+.

Features
LATEST MODEL
  • Broadcom processor - BCM2837B0, Cortex 64-bit SoC @1.4GHz
  • 2.4GHz and 5GHz IEEE 802.11.b/g/n/ac wireless LAN, Bluetooth 4.2/BLE
  • 512MB RAM
  • 1x USB 2.0 port
  • 40pin extended GPIO
  • HDMI, MIPI DSI display port, MIPI CSI camera port, 4 pole stereo output and composite video port
  • Extended 40-pin GPIO header
Buy now
Explore Community
See Videos, Pinouts, or Ask a Question
Raspberry Pi 3 Model B+
1GB RAM
The Raspberry Pi3 Model B+ is the latest product in the Raspberry Pi3 range, boasting a 64-Bit quad core processor running at 1.4GHz, dual band 2.4GHz / 5.0GHz wireless, Bluetooth 4.2/BLE, faster Ethernet and PoE capability via a separate PoE HAT.

The dual band wireless comes with modular compliance certification allowing the board to be designed into end product without the need for further wireless compliance testing, improving both cost and time to market.
Features
LATEST MODEL
Buy now
Explore Community
See Videos, Pinouts, or Ask a Question
Raspberry Pi 3 Model B
1GB RAM
Built on the latest Broadcom 2837 ARMv8 64bit processor, the new generation Raspberry Pi 3 Model B is faster and more powerful than its predecessors. With built-in wireless and Bluetooth connectivity, it becomes the ideal IoT ready solution.
Features
  • 1.2GHz QUAD Core Broadcom BCM2837 64bit ARMv8 processor
  • BCM43438 WiFi on board
  • Bluetooth Low Energy (BLE) on board
  • 1GB RAM
  • 4x USB 2 ports
  • 40pin extended GPIO
  • HDMI and RCA video output
Buy now
Explore Community
See Videos, Pinouts, or Ask a Question
Raspberry Pi 2 Model B v1.2
1GB RAM
The second generation Raspberry Pi model with enhanced features that render it capable of running a full range of ARM GNU/Linux distributions in addition to Microsoft Windows 10 IoT Core. Offering excellent flexibility for learners, it is an ideal option for school projects and is fully compatible with Raspberry Pi 1 devices.

The Raspberry Pi 2 Model B v1.2 requires the latest operating system for full functionality. Please download and install the latest version available from RaspberryPi.org/downloads onto your microSD card before booting.
Features
  • 900MHz QUAD Core Broadcom BCM2837 processor
  • 1GB RAM
  • 4x USB 2.0 ports
  • 40pin extended GPIO
  • HDMI and RCA video output
Raspberry Pi Compute Module 3+
1GB RAM
The Compute Module 3+ is the latest addition to the Raspberry Pi Computer Module range. Based on the same chip as Raspberry Pi 3 Model B+ Broadcom BCM2837B0, a 64-bit quad core processor running at 1.2GHz. The new Compute Model 3+ comes in three different memory variants; 8GB, 16GB & 32GB, to suits every kind of industrial embedded design applications.

Compute Module 3+ simplifies the design process engineers need to undertake when developing a System on Module (SoM) solution into their final product. Engineers do not need to concern themselves with the complexities of interfacing with the BCM2837B0 processer directly and instead can concentrate on designing the interfaces to their own IO board and their application software. This simplicity fosters rapid development.
Features
LATEST MODEL
  • Broadcom BCM2837B0, Cortex-A53 64-bit Soc @ 1.2GHz
  • 1Gbyte LPDDR2 SDRAM
  • Memory Options: 8Gbytes, 16Gbytes, 32Gbytes eMMC Flash
  • Multimedia: H.264, MPEG-4 decode (1080p30), H.264 encode (1080p30), OpenGL ES 1.1, 2.0 graphics
  • 35u hard gold plated IO Pins
Raspberry Pi Compute Module 3+ Lite
1GB RAM
The Compute Module 3+ Lite product is the same as the Compute Module 3+, within a 200 pin SODIMM design; except the eMMC Flash is not fitted, and the SD/eMMC interface pins are available for the user to connect their own SD/eMMC device to the Broadcom BCM2837B0 processor.

(N.B. when operating with the IO Board, an SD card with a suitable image must be connected to the IO board for the system to work).
Features
LATEST MODEL
  • Broadcom BCM2837B0, Cortex-A53 64-bit Soc @ 1.2GHz
  • 1Gbyte LPDDR2 SDRAM
  • Multimedia: H.264, MPEG-4 decode (1080p30), H.264 encode (1080p30), OpenGL ES 1.1, 2.0 graphics
  • 35u hard gold plated IO Pins
Raspberry Pi Compute Module 3
1GB RAM
The Compute Module 3, within a 200 pin SODIMM design, simplifies the design process engineers need to undertake when developing a System on Module (SoM) solution into their final product. Engineers do not need to concern themselves with the complexities of interfacing with the BCM2837 processer directly and instead can concentrate on designing the interfaces to their own IO board and their application software. This simplicity fosters rapid development.
Features
LATEST MODEL
  • Broadcom BCM2837 processor
  • 1Gbyte LPDDR2 RAM
  • 4Gbytes eMMC Flash
  • 35u hard gold plated IO Pins

Interested in this?

See the Compute Module Dev Kit as well

Find out more
Raspberry Pi Compute Module 3 Lite
1GB RAM
The Compute Module 3 Lite product is the same as the Compute Module 3, within a 200 pin SODIMM design; except the eMMC Flash is not fitted, and the SD/eMMC interface pins are available for the user to connect their own SD/eMMC deviceBroadcom BCM2837 processor.

(N.B. when operating with the IO Board, an SD card with a suitable image must be connected to the IO board for the system to work).
Features
LATEST MODEL
  • Broadcom BCM2837 processor
  • 35u hard gold plated IO Pins
  • 1Gbyte LPDDR2 RAM
Raspberry Pi Compute Module 1
512MB RAM
The original compute module 1 is based upon the BCM2835 chip. A SODIMM sized (6cm x 3.5cm) board with 4GB eMMC Flash memory making it more suitable for design-in.
Features
  • 700MHz Broadcom BCM2835 processor
  • 512MB RAM
  • 4GB eMMC Flash Memory
  • 6cm x 3.5cm SODIMM sized board

Interested in this?

See the Compute Module Dev Kit as well

Find out more

Earlier Generations of Raspberry Pi


See a comparison chart of all Pi Models

Raspberry Pi 1 Model A+
512MB RAM
An affordable model suitable for embedded and low-power projects that do not require Ethernet or multiple USB ports, the Raspberry Pi Model A+ boasts a 40 pin GPIO header, enhanced audio functionality and a small, neat design.
Features
  • 700MHz Broadcom BCM2835 processor
  • 512MB RAM
  • 1x USB 2.0 port
  • 40pin extended GPIO
  • HDMI and RCA video output
Raspberry Pi 1 Model B+
512MB RAM
The final iteration of the original Raspberry Pi series, the Model B+ boasts four USB 2.0 ports, low power consumption, a smooth push-push micro SD version and four squarely-placed mounting holes for a flexible, intuitive experience that optimises available space on the board.
Features
  • 700MHz Broadcom BCM2835 processor
  • 512MB RAM
  • 4x USB 2.0 ports
  • 40pin extended GPIO
  • HDMI and RCA video output
Raspberry Pi 1 Model B
512MB RAM
A high-spec iteration of the original Raspberry Pi 1, the Model B boasts 512MB of RAM, two USB ports and a 100MB Ethernet port, with a compact and space-optimising design suitable for a wide variety of applications for learners and experts alike.
Features
  • 700MHz Broadcom BCM2835 processor
  • 512MB RAM
  • 2x USB 2.0 ports
  • 26pin GPIO
  • HDMI and RCA video output

EXCLUSIVE Raspberry Pi Customisation Service

Custom versions of ANY Raspberry Pi board available for mass production
purposes with unique access to design & manufacturing services.

Customise my Pi

Raspberry Pi Projects and Ideas

Raspberry Pi Weather Station

This super-fun and easy to follow 20 minute kit project leverages the Internet of Things (IoT) using the new Raspberry Pi 3 with built-in WiFi, a Sense HAT, and the Initial State cloud platform.

Read more >

PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table

Follow this step by step guide on how to make a classic gaming table at minimal cost powered by Raspberry Pi 3.

Read more >

NoIR V2 - Video Streaming Baby Monitor

Capture low light stills and video using this the latest 8MP Sony lens camera from Raspberry Pi.

Read more >

Getting to know the Raspberry Pi Camera and Pi Noir

The Raspberry Pi is capable of many great things but one of the most accessible and rewarding is something incredibly simple, taking a photograph. We take this for granted as a camera comes with our cell phone...

Read more >

Ben Heck's Raspberry Pi Build Projects

Watch every Ben Heck Raspberry-Pi feature episode to learn and be entertained.

Watch video >

LED Coffee Table Hack for Your Home

Build a coffee table with RGB LEDs and Program in Python.

Read more >