A Smart Home can provide people with a comfortable, safe, power-saving and convenient life by enabling intercommunication amongst all household appliances. This includes lights, HVAC (Heating, Ventilation and Air Conditioning), TVs, computers, entertainment system, and security system. They can be controlled by a smart home control panel installed in house or through GSM/CDMA, Internet, and PSTN networks. Smart home systems are also called home automation, electronic home/e-home, or intelligent home.
[+MORE]
Sensors play an important role in smart home systems. The following sensors can be used for different purposes in contribution to making a smart house.
Temperature, humidity, light, and air pressure sensors constitute an intelligent environment monitoring network. This network works with HVAC, electric windows, and lighting system to control indoors temperature, humidity, and lighting intensity so as to make a comfortable environment.
To build a security system, various devices such as cameras, reed sensors, smoke detectors, PIR (Passive Infrared) sensors, and IR sensors are required. You can also include sounders in security systems. Alarm sounder is a low current consumption device suitable for close proximity signaling in fire and security applications. Cameras are made based on image sensors which are the core devices implement real-time video capture. Reed sensors can be installed on doors and windows to detect intrusion. Smoke sensors are used to detect if there is fire accident. PIR sensors are a kind of motion sensor, responsible for detecting intruder’s motion in a specified area. When any of these devices detects something unexpected, an alarm is triggered and is reported to the property owner and management staff.
PIR sensors are used as human body detectors for the purpose to turn on and turn off lights based on presence and absence of people. Light sensors detect intensity of natural light based on which lights in home will be turned off in daytime and turned on at night. The combination of PIR and light sensors can provide an intelligent lighting control.
As sensing and wireless communication technologies evolve continuously, MEMS sensors of smaller size and wireless sensor network have already been introduced into smart home systems.[-LESS]
Hover over the diagram blocks to view more recommended solutions.
| |
|
|
|
| |
|
MCP9800DM-PCTL Thermal Sensor Kit
Microchip
The MCP9800 Thermal Sensor PICtail™ Demo Board demonstrates how to interface the MCP9800 to a PICmicro(R) microcontroller using the PICkit™ 1 Flash Starter Kit as a platform. |
|
| |
|
XL_STAR S08
Freescale / element14
The XL_STAR board allows a user to develop, download and debug up to 64KBytes of 'C' or assembler object code for the MC9S08MM128 MCU using CodeWarrior for MCUs V6.3 Special Edition, a professional IDE, for just the cost of the board. Connected to the MM128 MCU, via I2C, is the MMA8451Q a three axes accelerometer. The board is pre-programmed with firmware that uses the MM128 MCU and MMA8451Q accelerometer to drive a star array of LEDs. |
|
| |
|
STEVAL-MKI062V2 INEMO MEMS Sensor Board
STMicroelectronics
The STEVAL-MKI062V2 is the second generation of the iNEMO™ module family. It combines accelerometers, gyroscopes and magnetometers with pressure and temperature sensors to provide 3-axis sensing of linear, angular and magnetic motion, complemented with temperature and barometer/altitude readings, representing the new ST 10-DOF (degrees of freedom) platform. |
|
| |
|
EK-H4 Humidity Evaluation Kit
Sensirion
The evaluation kit EK-H4 combines an easy-to-use plug-and-play system for sensor evaluation with a data logging equipment for simultaneous recording of humidity and temperature. |
|
| |
|
EK-H5 Humidity Evaluation Kit
Sensirion
The evaluation kit EK-H5 is a very simple system to test and evaluate Sensirion’s humidity and temperature sensors. |
|
|
| AVAGO TECHNOLOGIES |
Light Sensor |
Application Note - Test Setup for Ambient Light Sensor Testing(335 KB,PDF) |
AV01-0224EN |
APDS-900x |
Click here |
| IST |
Humidity Sensor |
LinPicco Humidity Module Application Notes |
|
LinPicco Humidity Module |
Click here |
| IST |
Humidity Sensor |
Humidity Circuit Application Notes |
|
|
Click here |
| IST |
Humidity Sensor |
Sensor Cable Extension Application Notes |
|
|
Click here |
| IST |
Humidity Sensor |
SMD Humidity Sensor Application Notes |
|
|
Click here |
| MICROCHIP |
Temperature Sensor |
Temperature Sensing Technologies |
AN679 |
|
Click here |
| MICROCHIP |
Temperature Sensor |
Interfacing the MCP9800 I2C Digital Temperature Sensor to a PICmicro Microcontroller |
AN988 |
|
Click here |
| MICROCHIP |
Temperature Sensor |
Temperature Sensor Design Guide |
DG4 |
|
Click here |
| MICROCHIP |
Temperature Sensor |
Analog Solutions for Automotive Applications Design Guide |
DG9 |
|
Click here |
| MICROCHIP |
Temperature Sensor |
IC Temperature Sensor Accuracy Compensation with a PICmicro Microcontroller |
AN1001 |
MCP9800/1/2/3 |
Click here |
| NATIONAL SEMICONDUCTOR |
Temperature Sensor |
LM34/LM35 Precision Monolithic Temperature Sensors |
AN-460 |
LM34/LM35 |
Click here |
| NATIONAL SEMICONDUCTOR |
Temperature Sensor |
IC Temperature Sensor Provides Thermocouple Cold-Junction Compensation |
AN-225 |
|
Click here |
| SENSIRION |
Sensor |
ESD, Latch-Up and EMC For SHTxx Humidity and Temperature Sensors |
|
SHTxx |
Click here |
| SENSIRION |
Sensor |
Non-Linearity compensation |
|
SHTxx |
Click here |
| TEXAS INSTRUMENTS |
Temperature Sensor |
Interfacing the MSP430 and TMP100 Temperature Sensor |
|
TMP100 |
Click here |
| Manufacturer |
Product Type
| White Paper Title
| URL |
| APTINA IMAGING |
Sensor |
Demo Kit Quick Start Guide |
MT9P031I12STCD ES |
MT9P031I12STC |
Click here |
| APTINA IMAGING |
Sensor |
MT9T031 Product Flyer |
MT9T031C12STCD ES |
MT9T031C12STC |
Click here |
| APTINA IMAGING |
Sensor |
MT9V131 Product Flyer |
MT9V131C12STCD ES |
MT9V131C12STC |
Click here |
| APTINA IMAGING |
Sensor |
MT9V131 Product Flyer |
MT9V131C12STCH ES |
MT9V131C12STC |
Click here |
| APTINA IMAGING |
Sensor |
MT9V135 Product Flyer |
MT9V135C12STCD ES |
MT9V135C12STC |
Click here |
| MICROCHIP |
Temperature Sensor |
MCP9800 Temperature Sensor PICtail Demo Board |
MCP9800DM-PCTL |
MCP9800 |
Click here |
| MICROCHIP |
Temperature Sensor |
MCP9800 Temperature Data Logger Demo Board |
MCP9800DM-DL |
MCP9800 |
Click here |
| SENSIRION |
Sensor |
Evaluation Kit EK-H4 for Humidity Sensors SHTxx |
EK-H4 |
SHTxx |
Click here |
| SENSIRION |
Sensor |
Evaluation Kit EK-H5 for Humidity Sensors SHT2x |
EK-H5 |
SHT2x |
Click here |
| TEXAS INSTRUMENTS |
Temperature Sensor |
TMP100EVM User's Guide(Rev.a) |
TMP100EVM |
TMP100NA |
Click here |
| HONEYWELL S&C |
Humidity Sensors |
Humidity Sensors |
|
Click here |
| MICROCHIP |
Smoke Detector |
RE46C190-3V Photo Smoke Detector IC |
RE46C190 |
Click here |
| MICROCHIP |
Smoke Detector |
RE46C165/6/7/8 Photo & RE46C162/3 Ion Smoke Detector Ics |
RE46C165/6/7/8 |
Click here |
| MICROCHIP |
Smoke Detector |
RE46C165/6/7/8 Photo & RE46C162/3 Ion Smoke Detector Ics |
RE46C165/6/7/8 |
Click here |
| MICROCHIP |
Smoke Detector |
RE46C190 - 3V Photo Smoke Detector IC |
RE46C190 |
Click here |
This is tab 5
This is tab 6