2013/05/24
 
 
 
Electronic Applications

APPLICATIONS

All the resources you need to bring your designs to life

Back to: Applications > Sensing > Intelligent CNC

Applications Home

New Products

Lighting

Alternative Energy

Instrumentation & Measurement

Wireless

Transportation

Defence & Aerospace

Sensing

Products

Sensors & Transducers

Solutions

Design Resources

Support

Robotics

Medical

Intelligent CNC

CNC Machines diagram

 Intelligent CNC (Intelligent Computer Numerical Control) machines increase processing accuracy and efficiency while relieving operators’ physical as well as psychological workload. Additionally, these machines are capable of detecting, diagnosing and correcting all sorts of errors during production, as well as providing solutions that are optimized for production.

[+MORE]

Comparing with non-intelligent CNC machines, intelligent CNC machines are equipped with intelligent control units in addition to motion control units. Intelligent control units utilize information from process monitoring sensor groups, expertise library, and neural network to automatically determine and correct process parameters such as cutting speed, depth and rate. Moreover, intelligent CNC machines can provide active vibration and heat compensation, safe guarding, voice indication, and remote maintenance.
 

A process monitoring sensor groups consist of accelerometers, RTDs (Resistance Temperature Detectors), image sensors, microphones, and position sensors. Accelerometers are used to detect vibration so that active vibration control can be achieved. RTDs detect temperature of the work-piece and cutting tools so as to realize thermal shielding in order to reduce thermal deformation. Image sensors are used for wear-out evaluation of cutting tools. Microphones collect noise generated by machines to help intelligent control unit determine vibration intensity and lubricating condition. Position sensors implement function of on-line measurement of work-pieces’ size. Certainly, intelligent CNC machines also have motion control units that include position sensors, rotary encoders, proximity switches, current sensors and pressure sensors to work with process monitoring sensor group and achieve powerful functions.
  

CNC machines are not only getting smarter, but also evolving towards green equipments that have higher speed and accuracy with flexibility and network communication capability.[-LESS]


Hover over the diagram blocks to view more recommended solutions.

Detects position and motor speed.
Click for full parts list

Measures the co-ordinates or dimension of the workpiece and tools.
Click for full parts list

Measures the co-ordinates or dimension of the workpiece and tools.
Click for full parts list

Used for motion control
Click for full parts list

Measures current/power consumption

aaaaa
ACS758ECB-
200U-PFF-T

ALLEGRO
MICROSYSTEMS
IR22771SPBF
IR22771SPBF
INTERNATIONAL
RECTIFIER
ACS711KLCTR-25AB-T
ACS711KLCTR-
25AB-T

ALLEGRO
MICROSYSTEMS

Click for full parts list

Detects vibration of the machine bed.

LSM330DL
LSM330DL
STMICROELECTRONICS
ADXL212AEZ
ADXL212AEZ
ANALOG DEVICES
MPU-6000
MPU-6000
INVENSENSE
Click for full parts list

Measures the temperature of tools and workpieces .
Click for full parts list

Inspects the wear and tear of the different tools.
Click for full parts list

Collects noise to diagnose vibration and lubrication.
Click for full parts list

Ensures the safety of the machine operator
Click for full parts list

Measure pressure levels in pneumatic or liquid control system

MPL3115A2
MPL3115A2
FREESCALE SEMICONDUCTOR
MPX4250AP
MPX4250AP
FREESCALE SEMICONDUCTOR
FREESCALE SEMICONDUCTOR
MPX4115A
MPX4115A
FREESCALE SEMICONDUCTOR

Click for full parts list

ADC

AD9608BCPZ-125
AD9608BCPZ-125
ANALOG DEVICES
aaaaa
LTC2157CUP-14#PBF
New LINEAR TECHNOLOGY

Click for full parts list

Microprocessor
Click for full parts list

Motor Driver

DRV8301DCA
DRV8301DCA
New TEXAS INSTRUMENTS
LV8080LP-TE-L-E
LV8080LP-TE-L-E
ON SEMICONDUCTOR
MTS2916A-HGC1
MTS2916A-HGC1
MICROCHIP

Click for full parts list

Human Machine Interface
Click for full parts list


Image Description  
 
XL_STAR S08
XL_STAR S08
Freescale / element14
The XL_STAR board allows a user to develop, download and debug up to 64KBytes of 'C' or assembler object code for the MC9S08MM128 MCU using CodeWarrior for MCUs V6.3 Special Edition, a professional IDE, for just the cost of the board. Connected to the MM128 MCU, via I2C, is the MMA8451Q a three axes accelerometer. The board is pre-programmed with firmware that uses the MM128 MCU and MMA8451Q accelerometer to drive a star array of LEDs.
s
 
ADIS16220/PCBZ Vibration Sensor
ADIS16220/PCBZ Vibration Sensor
Analog Devices
The ADIS16220 iSensor® is a digital vibration sensor that combines industry-leading iMEMS® sensing technology with signal processing, data capture, and a convenient serial peripheral interface (SPI).
s
 
MT9D131C12STCD ES
MT9D131C12STCD ES
Aptina Imaging
s
LEM Current Sensor Process & quality control, productivity gain: quality improvement and time savings thanks to current measurement  25102E Click here
LEM Current Sensor Electrical measurement in automation industry Click here
PEPPERL & FUCHS  Proximity  4 steps for selecting the appropriate proximity switch 0846A Click here
HAMLIN  Reed Switch Soldering Temperatures  AN115 Click here
KNOWLES ACOUSTICS  Microphone Transducer Signal Port Location Key AN1-Issue03 Click here
KNOWLES ACOUSTICS  Microphone A Passive Current Source for Two-Wire Microphones AN16-Issue01 Click here
IST RTD Assembly and application rules for 600℃ sensor elements Click here
IST RTD Wire assembly and extensions Click here
HONEYWELL S&C RTD Hot Film Anemometry Click here
FREESCALE SEMICONDUCTOR  Accelerometer How Many Bits are Enough? The Trade-off Between High Resolution and Low Power Using Oversampling Modes AN4075 MMA845X Click here
FREESCALE SEMICONDUCTOR  Accelerometer Offset Calibration of the MMA8451, 2, 3Q AN4069 MMA845X Click here
FREESCALE SEMICONDUCTOR  Accelerometer Data Manipulation and Basic Settings of the MMA8451, 2, 3Q AN4076 MMA845X Click here
Manufacturer Product Type AN Title AN Number Part Number URL
HONEYWELL S&C  Safety Switches Choosing Safety Switches  Click here
AVAGO TECHNOLOGIES  Rotary Encoder  
Simplifying BLDC Commutation and Feedback System  
Click here
AVAGO TECHNOLOGIES  Rotary Encoder  
Implementation of a DSP-based 20-bit High Resolution Quasi-Absolute Encoder for Low-Speed Feedback Control Applications 
Click here
ANALOG DEVICES  Accelerometer The Five Motion Sense:Using MEMS Inertial Sensing TO Transform Applications Click here
Manufacturer Product Type White Paper Title URL
ANALOG DEVICES  Accelerometer KIT, EVAL FOR ADXL335 ACCELEROMETERS  EVAL-ADXL335Z ADXL335 Click here
ANALOG DEVICES  Accelerometer Vibration Sensor Evaluation Board  ADIS16220/PCBZ  ADIS1622X Click here
FREESCALE SEMICONDUCTOR  Accelerometer 3-AXIS ACCEL, ZSTAR2 DEMO BOARD  RD3473MMA7360L  MMA7360 Click here
STMICROELECTRONICS  Accelerometer ACCELEROMETER KIT, ±2G/±6G  STEVAL-MKI005V1  LIS3LV02DL  Click here
STMICROELECTRONICS  Accelerometer ACCELEROMETER KIT, ±2G/±6G  STEVAL-MKI006V1  LIS302DL  Click here
APTINA IMAGING  Image Sensor Demo Kit Quick Start Guide MT9P031I12STCD ES  MT9P031I12STC Click here
APTINA IMAGING  Image Sensor MT9T031 Product Flyer MT9T031C12STCD ES MT9T031C12STC Click here
APTINA IMAGING  Image Sensor MT9V131 Product Flyer MT9V131C12STCD ES  MT9V131C12STC Click here
APTINA IMAGING  Image Sensor MT9V131 Product Flyer MT9V131C12STCH ES  MT9V131C12STC Click here
APTINA IMAGING  Image Sensor MT9V135 Product Flyer MT9V135C12STCD ES  MT9V135C12STC Click here
Manufacturer Product Type Evaluation Kits Title EVKs Part Number Part Number URL
AVAGO TECHNOLOGIES  Rotary Encoder Motor Control Solutions   Click here
BANNER ENGINEERING Light Curtain Safety Light Screen Resolution   Click here
BANNER ENGINEERING Light Curtain Machine Safeguarding Solutions Click here
LABFACILITY  RTD Thermocouple, resistance thermometer and thermistor theory and practice  Click here
ANALOG DEVICES  Accelerometer ADIS1636X iSensor® IMUs  ADIS1636X Click here
ANALOG DEVICES  Accelerometer Low g iMEMS® Accelerometers   Click here
FREESCALE SEMICONDUCTOR  Accelerometer Low-g Accelerometers Part 1 – Basic Knowledge of Accelerometers   Click here
HONEYWELL S&C Linear Position Position Sensor SPS-L075-HALS SPS-L075 Click here
HONEYWELL S&C Current Sensor Current Sensor Click here
Manufacturer Product Type Training Title Part Number URL
This is tab 6